LimitSwitchBuilder Class¶
-
class
NXOpen.Mechatronics.
LimitSwitchBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.LimitSwitch
builder.To create a new instance of this class, use
NXOpen.Mechatronics.LimitSwitchCollection.CreateLimitSwitchBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
EnableLowerLimit | Returns or sets the lower limit option. If the enable is true, then the physics object will be applied a lower limit. |
EnableUpperLimit | Returns or sets the upper limit option. If the enable is true, then the physics object will be applied an upper limit. |
LowerLimit | Returns the lower limit used to judge whether need to switch the state. |
Name | Returns or sets the name. |
PersistentTag | Returns or sets the Persistent Tag used in the physics object |
SelectedPhysicsObject | Returns the physics select. This can be a physics object. |
Tag | Returns the Tag for this object. |
UpperLimit | Returns the upper limit used to judge whether need to switch the state. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EnableLowerLimit¶
-
LimitSwitchBuilder.
EnableLowerLimit
¶ Returns or sets the lower limit option. If the enable is true, then the physics object will be applied a lower limit.
-------------------------------------
Getter Method
Signature
EnableLowerLimit
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableLowerLimit
Parameters: enable (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableUpperLimit¶
-
LimitSwitchBuilder.
EnableUpperLimit
¶ Returns or sets the upper limit option. If the enable is true, then the physics object will be applied an upper limit.
-------------------------------------
Getter Method
Signature
EnableUpperLimit
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableUpperLimit
Parameters: enable (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerLimit¶
-
LimitSwitchBuilder.
LowerLimit
¶ Returns the lower limit used to judge whether need to switch the state.
-------------------------------------
Getter Method
Signature
LowerLimit
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PersistentTag¶
-
LimitSwitchBuilder.
PersistentTag
¶ Returns or sets the Persistent Tag used in the physics object
-------------------------------------
Getter Method
Signature
PersistentTag
Returns: Return type: int New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PersistentTag
Parameters: persistentTag (int) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectedPhysicsObject¶
-
LimitSwitchBuilder.
SelectedPhysicsObject
¶ Returns the physics select. This can be a physics object.
-------------------------------------
Getter Method
Signature
SelectedPhysicsObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperLimit¶
-
LimitSwitchBuilder.
UpperLimit
¶ Returns the upper limit used to judge whether need to switch the state.
-------------------------------------
Getter Method
Signature
UpperLimit
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
LimitSwitchBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.