HydraulicCylinderBuilder Class¶
-
class
NXOpen.Mechatronics.
HydraulicCylinderBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.HydraulicCylinder
builder.To create a new instance of this class, use
NXOpen.Mechatronics.HydraulicCylinderCollection.CreateHydraulicCylinderBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AxisJoint | Returns the Axis Joint. This can be a PhysicsJoint . |
Name | Returns or sets the name. |
PistonDiameter | Returns the diameter of the piston. |
PistonRodDiameter | Returns the diameter of the piston rod. |
PressureA | Returns the initial pressure of chamber A. |
PressureB | Returns the initial pressure of chamber B. |
RodType | Returns or sets the rod type. |
StrokeLength | Returns the overall stroke length of the cylinder. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HydraulicCylinderBuilderOutputRodType Enumeration | the Rod types. |
Property Detail¶
AxisJoint¶
-
HydraulicCylinderBuilder.
AxisJoint
¶ Returns the Axis Joint. This can be a
PhysicsJoint
.-------------------------------------
Getter Method
Signature
AxisJoint
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PistonDiameter¶
-
HydraulicCylinderBuilder.
PistonDiameter
¶ Returns the diameter of the piston.
-------------------------------------
Getter Method
Signature
PistonDiameter
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PistonRodDiameter¶
-
HydraulicCylinderBuilder.
PistonRodDiameter
¶ Returns the diameter of the piston rod.
-------------------------------------
Getter Method
Signature
PistonRodDiameter
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PressureA¶
-
HydraulicCylinderBuilder.
PressureA
¶ Returns the initial pressure of chamber A.
-------------------------------------
Getter Method
Signature
PressureA
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PressureB¶
-
HydraulicCylinderBuilder.
PressureB
¶ Returns the initial pressure of chamber B.
-------------------------------------
Getter Method
Signature
PressureB
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RodType¶
-
HydraulicCylinderBuilder.
RodType
¶ Returns or sets the rod type.
-------------------------------------
Getter Method
Signature
RodType
Returns: Return type: NXOpen.Mechatronics.HydraulicCylinderBuilderOutputRodType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RodType
Parameters: rodType ( NXOpen.Mechatronics.HydraulicCylinderBuilderOutputRodType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StrokeLength¶
-
HydraulicCylinderBuilder.
StrokeLength
¶ Returns the overall stroke length of the cylinder.
-------------------------------------
Getter Method
Signature
StrokeLength
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
HydraulicCylinderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.