GraphControlCollection Class

class NXOpen.Mechatronics.GraphControlCollection

Bases: object

Represents a collection of Graph Control.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX8.0.0.

Methods

Method Description
CreateGraphControlBuilder Creates a NXOpen.Mechatronics.GraphControlBuilder.
FindObject Finds the NXOpen.Mechatronics.GraphControl with the given name.

Method Detail

CreateGraphControlBuilder

GraphControlCollection.CreateGraphControlBuilder

Creates a NXOpen.Mechatronics.GraphControlBuilder.

Signature CreateGraphControlBuilder(graphControl)

Parameters:graphControl (NXOpen.Mechatronics.GraphControl) – NXOpen.Mechatronics.GraphControl to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.GraphControlBuilder

New in version NX8.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

GraphControlCollection.FindObject

Finds the NXOpen.Mechatronics.GraphControl with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.GraphControl.
Returns:NXOpen.Mechatronics.GraphControl with this name.
Return type:NXOpen.Mechatronics.GraphControl

New in version NX8.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)