GanttOperationBuilderSimpleOperationType Enumeration

NXOpen.Mechatronics.GanttOperationBuilder.SimpleOperationType is an alias for NXOpen.Mechatronics.GanttOperationBuilderSimpleOperationType

class NXOpen.Mechatronics.GanttOperationBuilderSimpleOperationType

Bases: object

the pause operation Type enum

Enum Members

Enum Member Enum Member Description
Simple
Pause
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.