ForceTorqueControlCollection Class¶
-
class
NXOpen.Mechatronics.
ForceTorqueControlCollection
¶ Bases:
object
Represents the ForceTorque collection for ForceTorque constraint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateForceTorqueControlBuilder | Creates a NXOpen.Mechatronics.ForceTorqueControlBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ForceTorqueControl with the given name. |
Method Detail¶
CreateForceTorqueControlBuilder¶
-
ForceTorqueControlCollection.
CreateForceTorqueControlBuilder
¶ Creates a
NXOpen.Mechatronics.ForceTorqueControlBuilder
.Signature
CreateForceTorqueControlBuilder(forceControl)
Parameters: forceControl ( NXOpen.Mechatronics.ForceTorqueControl
) –NXOpen.Mechatronics.ForceTorqueControl
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ForceTorqueControlBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ForceTorqueControlCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ForceTorqueControl
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.SpeedControl
.Returns: NXOpen.Mechatronics.ForceTorqueControl
with this name.Return type: NXOpen.Mechatronics.ForceTorqueControl
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)