FixedJointCollection Class

class NXOpen.Mechatronics.FixedJointCollection

Bases: object

Represents a collection of Fixed Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Methods

Method Description
CreateFixedJointBuilder Creates a NXOpen.Mechatronics.FixedJointBuilder.
FindObject Finds the NXOpen.Mechatronics.FixedJoint with the given name.

Method Detail

CreateFixedJointBuilder

FixedJointCollection.CreateFixedJointBuilder

Creates a NXOpen.Mechatronics.FixedJointBuilder.

Signature CreateFixedJointBuilder(slide)

Parameters:slide (NXOpen.Mechatronics.FixedJoint) – NXOpen.Mechatronics.FixedJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.FixedJointBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

FixedJointCollection.FindObject

Finds the NXOpen.Mechatronics.FixedJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.FixedJoint.
Returns:NXOpen.Mechatronics.FixedJoint with this name.
Return type:NXOpen.Mechatronics.FixedJoint

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)