ExternalSignalConfigurationCollection Class¶
-
class
NXOpen.Mechatronics.
ExternalSignalConfigurationCollection
¶ Bases:
object
Represents a collection of ExternalSignalConfigurationObject.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateExternalSignalConfigurationBuilder | Creates a NXOpen.Mechatronics.ExternalSignalConfigurationBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ExternalSignalConfigurationObject with the given name. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateExternalSignalConfigurationBuilder¶
-
ExternalSignalConfigurationCollection.
CreateExternalSignalConfigurationBuilder
¶ Creates a
NXOpen.Mechatronics.ExternalSignalConfigurationBuilder
.Signature
CreateExternalSignalConfigurationBuilder(externalSignalConfigurationObject)
Parameters: externalSignalConfigurationObject ( NXOpen.Mechatronics.ExternalSignalConfigurationObject
) –NXOpen.Mechatronics.ExternalSignalConfigurationObject
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ExternalSignalConfigurationBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ExternalSignalConfigurationCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ExternalSignalConfigurationObject
with the given name. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ExternalSignalConfigurationObject
.Returns: NXOpen.Mechatronics.ExternalSignalConfigurationObject
with this name.Return type: NXOpen.Mechatronics.ExternalSignalConfigurationObject
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)