ExternalConnectionElementBuilderConditionType Enumeration¶
NXOpen.Mechatronics.ExternalConnectionElementBuilder.ConditionType is an alias for NXOpen.Mechatronics.ExternalConnectionElementBuilderConditionType
-
class
NXOpen.Mechatronics.
ExternalConnectionElementBuilderConditionType
¶ Bases:
object
the condition type.
Enum Members
Enum Member Enum Member Description Eq equal Gt greater than Lt less than Ge greater than or equal Le less than or equal Ne not equal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-