ExpressionBlockFormulaCollection Class

class NXOpen.Mechatronics.ExpressionBlockFormulaCollection

Bases: object

Represents a collection of ExpressionBlock Formula.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX11.0.0.

Method Detail

CreateExpressionBlockFormulaBuilder

ExpressionBlockFormulaCollection.CreateExpressionBlockFormulaBuilder

Creates a NXOpen.Mechatronics.ExpressionBlockFormulaBuilder.

Signature CreateExpressionBlockFormulaBuilder(expressionBlockFormula)

Parameters:expressionBlockFormula (NXOpen.Mechatronics.ExpressionBlockFormula) – NXOpen.Mechatronics.ExpressionBlockFormula to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.ExpressionBlockFormulaBuilder

New in version NX11.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

ExpressionBlockFormulaCollection.FindObject

Finds the NXOpen.Mechatronics.ExpressionBlockFormula with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.ExpressionBlockFormula.
Returns:NXOpen.Mechatronics.ExpressionBlockFormula with this name.
Return type:NXOpen.Mechatronics.ExpressionBlockFormula

New in version NX11.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)