ElectricalPartCollection Class¶
-
class
NXOpen.Mechatronics.
ElectricalPartCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.ElectricalPartCollection
To obtain an instance of this class, refer to
NXOpen.Mechatronics.MechatronicsManager
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CreateElectricalPartBuilder | Create builder for ElectricalPart class |
FindObject | Finds the NXOpen.Mechatronics.ElectricalPart object with the given name. |
Method Detail¶
CreateElectricalPartBuilder¶
-
ElectricalPartCollection.
CreateElectricalPartBuilder
¶ Create builder for ElectricalPart class
Signature
CreateElectricalPartBuilder(object)
Parameters: object ( NXOpen.Mechatronics.ElectricalPart
) –NXOpen.Mechatronics.ElectricalPart
to be edited, if None then create a new oneReturns: NXOpen.Mechatronics.ElectricalPart
objectReturn type: NXOpen.Mechatronics.ElectricalPartBuilder
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ElectricalPartCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ElectricalPart
object with the given name.Signature
FindObject(name)
Parameters: name (str) – Name of the object, actually it shall be handle. Returns: NXOpen.Mechatronics.ElectricalPart
object with this name.Return type: NXOpen.Mechatronics.ElectricalPart
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)