ECADImportBuilderPositionMode Enumeration¶
NXOpen.Mechatronics.ECADImportBuilder.PositionMode is an alias for NXOpen.Mechatronics.ECADImportBuilderPositionMode
-
class
NXOpen.Mechatronics.
ECADImportBuilderPositionMode
¶ Bases:
object
Represents the position mode.
Deprecated since version NX9.0.0: This enum type has no replacement. It is no longer supported.
Enum Members
Enum Member Enum Member Description InferredOnly Inferred Only AbsoluteOrigin Absolute Origin SelectOrigin Select Origin ByConstraints By Constraints Move Move -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-