DynamicObjectTableBuilder Class¶
-
class
NXOpen.Mechatronics.
DynamicObjectTableBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.DynamicObjectTableBuilder
builder.DynamicObjectTableBuilder is used to maintain the
NXOpen.Mechatronics.DynamicObjectTable
which is used for dynamic object instantiation.To create a new instance of this class, use
NXOpen.Mechatronics.DynamicObjectTableCollection.CreateDynamicObjectTableBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetInstances | Gets all Instances. |
GetObject | Returns the object currently being edited by this builder. |
SetInstances | Sets all Instances. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
DynamicObjectTableBuilderInstance_Struct Struct |
|
Property Detail¶
Name¶
-
DynamicObjectTableBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetInstances¶
-
DynamicObjectTableBuilder.
GetInstances
¶ Gets all Instances.
Signature
GetInstances()
Returns: Array of Instances Return type: list of NXOpen.Mechatronics.DynamicObjectTableBuilderInstance_Struct
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetInstances¶
-
DynamicObjectTableBuilder.
SetInstances
¶ Sets all Instances.
Each Instance name must be unique in the context of input Instance list. Or the builder will raise an exception.
Signature
SetInstances(instances)
Parameters: instances (list of NXOpen.Mechatronics.DynamicObjectTableBuilderInstance_Struct
) – Array of InstancesNew in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
DynamicObjectTableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.