DistanceSensorCollection Class¶
-
class
NXOpen.Mechatronics.
DistanceSensorCollection
¶ Bases:
object
Represents a collection of Distance Sensor.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateDistanceSensorBuilder | Creates a NXOpen.Mechatronics.DistanceSensorBuilder . |
FindObject | Finds the NXOpen.Mechatronics.DistanceSensor with the given name. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateDistanceSensorBuilder¶
-
DistanceSensorCollection.
CreateDistanceSensorBuilder
¶ Creates a
NXOpen.Mechatronics.DistanceSensorBuilder
.Signature
CreateDistanceSensorBuilder(distanceSensor)
Parameters: distanceSensor ( NXOpen.Mechatronics.DistanceSensor
) –NXOpen.Mechatronics.DistanceSensor
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.DistanceSensorBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
DistanceSensorCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.DistanceSensor
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.DistanceSensor
.Returns: NXOpen.Mechatronics.DistanceSensor
with this name.Return type: NXOpen.Mechatronics.DistanceSensor
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)