DisplayChangerCollection Class

class NXOpen.Mechatronics.DisplayChangerCollection

Bases: object

Represents a collection of Object Transformer.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX10.0.0.

Method Detail

CreateDisplayChangerBuilder

DisplayChangerCollection.CreateDisplayChangerBuilder

Creates a NXOpen.Mechatronics.DisplayChangerBuilder.

Signature CreateDisplayChangerBuilder(objectSrc)

Parameters:objectSrc (NXOpen.Mechatronics.DisplayChanger) – NXOpen.Mechatronics.DisplayChanger to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.DisplayChangerBuilder

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

DisplayChangerCollection.FindObject

Finds the NXOpen.Mechatronics.DisplayChanger with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.DisplayChanger.
Returns:NXOpen.Mechatronics.DisplayChanger with this name.
Return type:NXOpen.Mechatronics.DisplayChanger

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)