ComparisonResultElectricalPartStatus Enumeration¶
NXOpen.Mechatronics.ComparisonResultElectricalPart.Status is an alias for NXOpen.Mechatronics.ComparisonResultElectricalPartStatus
-
class
NXOpen.Mechatronics.
ComparisonResultElectricalPartStatus
¶ Bases:
object
Defines statuses of electrical parts
Enum Members
Enum Member Enum Member Description Added Added status Removed Removed status Updated Updated status Identical Identical status -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-