CollisionMaterialCollection Class

class NXOpen.Mechatronics.CollisionMaterialCollection

Bases: object

Represents a collection of Collision Material.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Method Detail

CreateCollisionMaterialBuilder

CollisionMaterialCollection.CreateCollisionMaterialBuilder

Creates a NXOpen.Mechatronics.CollisionMaterialBuilder.

Signature CreateCollisionMaterialBuilder(collisionMaterial)

Parameters:collisionMaterial (NXOpen.Mechatronics.CollisionMaterial) – NXOpen.Mechatronics.CollisionMaterial to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.CollisionMaterialBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

CollisionMaterialCollection.FindObject

Finds the NXOpen.Mechatronics.CollisionMaterial with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.CollisionMaterial.
Returns:NXOpen.Mechatronics.CollisionMaterial with this name.
Return type:NXOpen.Mechatronics.CollisionMaterial

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)