CollisionBodyCollection Class¶
-
class
NXOpen.Mechatronics.
CollisionBodyCollection
¶ Bases:
object
Represents a collection of Collision Bodies.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateCollisionBodyBuilder | Creates a NXOpen.Mechatronics.CollisionBodyBuilder . |
FindObject | Finds the NXOpen.Mechatronics.CollisionBody with the given name. |
Method Detail¶
CreateCollisionBodyBuilder¶
-
CollisionBodyCollection.
CreateCollisionBodyBuilder
¶ Creates a
NXOpen.Mechatronics.CollisionBodyBuilder
.Signature
CreateCollisionBodyBuilder(collideBody)
Parameters: collideBody ( NXOpen.Mechatronics.CollisionBody
) –NXOpen.Mechatronics.CollisionBody
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.CollisionBodyBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
CollisionBodyCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.CollisionBody
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.CollisionBody
.Returns: NXOpen.Mechatronics.CollisionBody
with this name.Return type: NXOpen.Mechatronics.CollisionBody
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)