CamProfileCollection Class¶
-
class
NXOpen.Mechatronics.
CamProfileCollection
¶ Bases:
object
Represents a collection of Cam Profile.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CreateCamProfileBuilder | Creates a NXOpen.Mechatronics.CamProfileBuilder . |
FindObject | Finds the NXOpen.Mechatronics.CamProfile with the given name. |
Method Detail¶
CreateCamProfileBuilder¶
-
CamProfileCollection.
CreateCamProfileBuilder
¶ Creates a
NXOpen.Mechatronics.CamProfileBuilder
.Signature
CreateCamProfileBuilder(segmentTable)
Parameters: segmentTable ( NXOpen.Mechatronics.CamProfile
) –NXOpen.Mechatronics.CamProfile
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.CamProfileBuilder
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
CamProfileCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.CamProfile
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.CamProfile
.Returns: NXOpen.Mechatronics.CamProfile
with this name.Return type: NXOpen.Mechatronics.CamProfile
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)