CamProfileBuilderSlaveValueUnit Enumeration¶
NXOpen.Mechatronics.CamProfileBuilder.SlaveValueUnit is an alias for NXOpen.Mechatronics.CamProfileBuilderSlaveValueUnit
-
class
NXOpen.Mechatronics.
CamProfileBuilderSlaveValueUnit
¶ Bases:
object
The master value unit indicates which type master joint is.
Enum Members
Enum Member Enum Member Description LinearPosition Linear Position RotaryPosition Rotary Position LinearSpeed Linear Speed RotarySpeed Rotary Speed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-