CamProfileBuilderProfileCyclicType Enumeration¶
NXOpen.Mechatronics.CamProfileBuilder.ProfileCyclicType is an alias for NXOpen.Mechatronics.CamProfileBuilderProfileCyclicType
-
class
NXOpen.Mechatronics.
CamProfileBuilderProfileCyclicType
¶ Bases:
object
Indicates which cyclic type should be take.The type of Cam Profile can be switched between non-cyclic, cyclic and relative cyclic
Enum Members
Enum Member Enum Member Description RelativeCyclic In Relative Cyclic Cam Profiles the start point and end point of the profile do not necessarily have to be equal. Cyclic In Cyclic Cam Profiles the points at the beginning and the end of the Master Axis range need to be identical with respect to Slave Axis value, slope and curve. NonCyclic Non-cyclic Cam Profiles are defined only in the defined master axis range. Exceeding this range will cause an error. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-