BallJointCollection Class

class NXOpen.Mechatronics.BallJointCollection

Bases: object

Represents a collection of Ball Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Methods

Method Description
CreateBallJointBuilder Creates a NXOpen.Mechatronics.BallJointBuilder.
FindObject Finds the NXOpen.Mechatronics.BallJoint with the given name.

Method Detail

CreateBallJointBuilder

BallJointCollection.CreateBallJointBuilder

Creates a NXOpen.Mechatronics.BallJointBuilder.

Signature CreateBallJointBuilder(slide)

Parameters:slide (NXOpen.Mechatronics.BallJoint) – NXOpen.Mechatronics.BallJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.BallJointBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

BallJointCollection.FindObject

Finds the NXOpen.Mechatronics.BallJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.BallJoint.
Returns:NXOpen.Mechatronics.BallJoint with this name.
Return type:NXOpen.Mechatronics.BallJoint

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)