AngularSpringJointCollection Class

class NXOpen.Mechatronics.AngularSpringJointCollection

Bases: object

Represents a collection of Angular Spring Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Method Detail

CreateAngularSpringJointBuilder

AngularSpringJointCollection.CreateAngularSpringJointBuilder

Creates a NXOpen.Mechatronics.AngularSpringJointBuilder.

Signature CreateAngularSpringJointBuilder(angularSpring)

Parameters:angularSpring (NXOpen.Mechatronics.AngularSpringJoint) – NXOpen.Mechatronics.AngularSpringJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.AngularSpringJointBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

AngularSpringJointCollection.FindObject

Finds the NXOpen.Mechatronics.AngularSpringJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.AngularSpringJoint.
Returns:NXOpen.Mechatronics.AngularSpringJoint with this name.
Return type:NXOpen.Mechatronics.AngularSpringJoint

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)