AlignBodyCollection Class¶
-
class
NXOpen.Mechatronics.
AlignBodyCollection
¶ Bases:
object
Represents a collection of Align Body.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateAlignBodyBuilder | Creates a NXOpen.Mechatronics.AlignBodyBuilder . |
FindObject | Finds the NXOpen.Mechatronics.AlignBody with the given name. |
Method Detail¶
CreateAlignBodyBuilder¶
-
AlignBodyCollection.
CreateAlignBodyBuilder
¶ Creates a
NXOpen.Mechatronics.AlignBodyBuilder
.Signature
CreateAlignBodyBuilder(snapPoint)
Parameters: snapPoint ( NXOpen.Mechatronics.AlignBody
) –NXOpen.Mechatronics.AlignBody
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.AlignBodyBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
AlignBodyCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.AlignBody
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.AlignBody
.Returns: NXOpen.Mechatronics.AlignBody
with this name.Return type: NXOpen.Mechatronics.AlignBody
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)