AdapterSignalCollection Class

class NXOpen.Mechatronics.AdapterSignalCollection

Bases: object

Represents a collection of Adapter Signal.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX8.5.0.

Methods

Method Description
CreateAdapterSignalBuilder Creates a NXOpen.Mechatronics.AdapterSignalBuilder.
FindObject Finds the NXOpen.Mechatronics.AdapterSignal with the given name.

Method Detail

CreateAdapterSignalBuilder

AdapterSignalCollection.CreateAdapterSignalBuilder

Creates a NXOpen.Mechatronics.AdapterSignalBuilder.

Signature CreateAdapterSignalBuilder(object)

Parameters:object (NXOpen.Mechatronics.AdapterSignal) – NXOpen.Mechatronics.AdapterSignal to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.AdapterSignalBuilder

New in version NX8.5.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

AdapterSignalCollection.FindObject

Finds the NXOpen.Mechatronics.AdapterSignal with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.AdapterSignal.
Returns:NXOpen.Mechatronics.AdapterSignal with this name.
Return type:NXOpen.Mechatronics.AdapterSignal

New in version NX8.5.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)