AccelerometerBuilder Class¶
-
class
NXOpen.Mechatronics.
AccelerometerBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.Accelerometer
builder.To create a new instance of this class, use
NXOpen.Mechatronics.AccelerometerCollection.CreateAccelerometerBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
LowerAngularTrimRange | Returns the lower angular trim range used to trim the Accelerometer data. |
LowerOutputRange | Returns the lower output range used to scale the Accelerometer data. Its measure type contains constant, voltage, current |
LowerTrimRange | Returns the lower trim range used to trim the Accelerometer data. |
MeasureType | Returns or sets the measure type. |
Name | Returns or sets the name. |
RigidBody | Returns the Rigid Body. This can be a NXOpen.Mechatronics.RigidBody . |
Tag | Returns the Tag for this object. |
UpperAngularTrimRange | Returns the upper angular trim range used to trim the Accelerometer data. |
UpperOutputRange | Returns the upper output range used to scale the Accelerometer data. |
UpperTrimRange | Returns the upper trim range used to trim the Accelerometer data. |
UseScale | Returns or sets the use scale flag, which is used to control if the accelerometer includes scale parameters. |
UseTrim | Returns or sets the use trim flag, which is used to control if the accelerometer includes trim parameters. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AccelerometerBuilderOutputMeasureType Enumeration | the Measure types. |
Property Detail¶
LowerAngularTrimRange¶
-
AccelerometerBuilder.
LowerAngularTrimRange
¶ Returns the lower angular trim range used to trim the Accelerometer data.
-------------------------------------
Getter Method
Signature
LowerAngularTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerOutputRange¶
-
AccelerometerBuilder.
LowerOutputRange
¶ Returns the lower output range used to scale the Accelerometer data. Its measure type contains constant, voltage, current
-------------------------------------
Getter Method
Signature
LowerOutputRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerTrimRange¶
-
AccelerometerBuilder.
LowerTrimRange
¶ Returns the lower trim range used to trim the Accelerometer data.
-------------------------------------
Getter Method
Signature
LowerTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MeasureType¶
-
AccelerometerBuilder.
MeasureType
¶ Returns or sets the measure type.
-------------------------------------
Getter Method
Signature
MeasureType
Returns: Return type: NXOpen.Mechatronics.AccelerometerBuilderOutputMeasureType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MeasureType
Parameters: measureType ( NXOpen.Mechatronics.AccelerometerBuilderOutputMeasureType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RigidBody¶
-
AccelerometerBuilder.
RigidBody
¶ Returns the Rigid Body. This can be a
NXOpen.Mechatronics.RigidBody
.-------------------------------------
Getter Method
Signature
RigidBody
Returns: Return type: NXOpen.Mechatronics.SelectRigidBody
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperAngularTrimRange¶
-
AccelerometerBuilder.
UpperAngularTrimRange
¶ Returns the upper angular trim range used to trim the Accelerometer data.
-------------------------------------
Getter Method
Signature
UpperAngularTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperOutputRange¶
-
AccelerometerBuilder.
UpperOutputRange
¶ Returns the upper output range used to scale the Accelerometer data.
-------------------------------------
Getter Method
Signature
UpperOutputRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperTrimRange¶
-
AccelerometerBuilder.
UpperTrimRange
¶ Returns the upper trim range used to trim the Accelerometer data.
-------------------------------------
Getter Method
Signature
UpperTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseScale¶
-
AccelerometerBuilder.
UseScale
¶ Returns or sets the use scale flag, which is used to control if the accelerometer includes scale parameters.
-------------------------------------
Getter Method
Signature
UseScale
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseScale
Parameters: useScale (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseTrim¶
-
AccelerometerBuilder.
UseTrim
¶ Returns or sets the use trim flag, which is used to control if the accelerometer includes trim parameters.
-------------------------------------
Getter Method
Signature
UseTrim
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseTrim
Parameters: useTrim (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
AccelerometerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.