TransformBlockBuilderTransformtype Enumeration¶
NXOpen.MechanicalRouting.TransformBlockBuilder.Transformtype is an alias for NXOpen.MechanicalRouting.TransformBlockBuilderTransformtype
-
class
NXOpen.MechanicalRouting.
TransformBlockBuilderTransformtype
¶ Bases:
object
Specifies the options available for transform. The available opitons are Manipulator, OrientXpress, View, Plane, Vector.
Enum Members
Enum Member Enum Member Description NotSet OrientXpress OrientXpress allows you to move a point constrained to a coordinate axis or plane in wcs. Vector Vector allows you to move a point constrained to a specified direction. View View allows you to move a point constrained to a plane, normal to the view. Manipulator Manipulator allows you to move a point dynamically to any location in wcs. Plane Plane allows you to move a point constrained to a specified plane. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-