PathStockPreferenceBuilderAssignStockSubType Enumeration¶
NXOpen.MechanicalRouting.PathStockPreferenceBuilder.AssignStockSubType is an alias for NXOpen.MechanicalRouting.PathStockPreferenceBuilderAssignStockSubType
-
class
NXOpen.MechanicalRouting.
PathStockPreferenceBuilderAssignStockSubType
¶ Bases:
object
Determines the type of sub stock being assigned. This is only valid when Stock type is ‘Stock’
Enum Members
Enum Member Enum Member Description Stock Default stock subtype. SpaceReservation Space Reservation stock subtype. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-