PathStockPreferenceBuilderAssignMethod Enumeration¶
NXOpen.MechanicalRouting.PathStockPreferenceBuilder.AssignMethod is an alias for NXOpen.MechanicalRouting.PathStockPreferenceBuilderAssignMethod
-
class
NXOpen.MechanicalRouting.
PathStockPreferenceBuilderAssignMethod
¶ Bases:
object
Determines how to choose which stock to assign.
Deprecated since version NX11.0.1: Use
NXOpen.MechanicalRouting.PathStockPreferenceBuilderStockMethod
instead.Enum Members
Enum Member Enum Member Description NotSet No Stock. FromStartObject Finds a stock based off of the default stock and the object selected by the user. Circular User specified diameter, creates round space reservation stock. Rectangular User specified values, creates rectangular space reservation stock. FlatOval User specified values, creates flat_oval space reservation stock. SpecifiedStock Stock selected from Specify Item dialog -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-