PartPlacementBuilderPlacementValidationStatus Enumeration¶
NXOpen.MechanicalRouting.PartPlacementBuilder.PlacementValidationStatus is an alias for NXOpen.MechanicalRouting.PartPlacementBuilderPlacementValidationStatus
-
class
NXOpen.MechanicalRouting.
PartPlacementBuilderPlacementValidationStatus
¶ Bases:
object
The placement validation status
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Success part placement is successful as expected PartNotConnectedToRout after placement connection should have been built with routing system but it was not -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-