MovePathBuilderDetachTypes Enumeration¶
NXOpen.MechanicalRouting.MovePathBuilder.DetachTypes is an alias for NXOpen.MechanicalRouting.MovePathBuilderDetachTypes
-
class
NXOpen.MechanicalRouting.
MovePathBuilderDetachTypes
¶ Bases:
object
Specifies the options that will allow the user to enforce the transformation by detaching the routing objects (if necessary) from objects that stop the selected object from moving.
Enum Members
Enum Member Enum Member Description AlwaysMaintainConnections AllowDetachOnConflict DetachSelectedObjects -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-