ManageInlineBehaviorBuilder Class¶
-
class
NXOpen.MechanicalRouting.
ManageInlineBehaviorBuilder
¶ Bases:
NXOpen.Builder
Represents
NXOpen.MechanicalRouting.ManageInlineBehaviorBuilder
.To create a new instance of this class, use
NXOpen.MechanicalRouting.BuilderFactory.CreateManageInlineBehaviorBuilder()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetInlineBehavior | Returns true if current model element revision as inline design element. |
GetObject | Returns the object currently being edited by this builder. |
SetInlineBehavior | Sets true to mark current model element revision as inline design element(which moves along with connected routing design elements), false for non-inline design element (which has its own position and drives connected routing design elements. |
SetModelElementRevision | Sets NXOpen.PDM.ModelElementRevision of Routing Reuse type. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetInlineBehavior¶
-
ManageInlineBehaviorBuilder.
GetInlineBehavior
¶ Returns true if current model element revision as inline design element.
Signature
GetInlineBehavior()
Returns: Return type: bool New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetInlineBehavior¶
-
ManageInlineBehaviorBuilder.
SetInlineBehavior
¶ Sets true to mark current model element revision as inline design element(which moves along with connected routing design elements), false for non-inline design element (which has its own position and drives connected routing design elements.
Its position is never driven by inline design elements). Client should call update after this as model element revision has been logged to change.
Signature
SetInlineBehavior(isInline)
Parameters: isInline (bool) – New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetModelElementRevision¶
-
ManageInlineBehaviorBuilder.
SetModelElementRevision
¶ Sets
NXOpen.PDM.ModelElementRevision
of Routing Reuse type.Raise an error if passed other type of object.
Signature
SetModelElementRevision(modelElementRevision)
Parameters: modelElementRevision ( NXOpen.PDM.ModelElementRevision
) –New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
ManageInlineBehaviorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.