InsulationBuilderWrapType Enumeration¶
NXOpen.MechanicalRouting.InsulationBuilder.WrapType is an alias for NXOpen.MechanicalRouting.InsulationBuilderWrapType
-
class
NXOpen.MechanicalRouting.
InsulationBuilderWrapType
¶ Bases:
object
The application type for wrapped Insulation
Enum Members
Enum Member Enum Member Description NoWarp No wrapping OverlapSpiral Overlap Spiral StripedSpiral Striped Spiral -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-