EditPointBuilderMotiontype Enumeration¶
NXOpen.MechanicalRouting.EditPointBuilder.Motiontype is an alias for NXOpen.MechanicalRouting.EditPointBuilderMotiontype
-
class
NXOpen.MechanicalRouting.
EditPointBuilderMotiontype
¶ Bases:
object
Specifies the options available for motion.
Enum Members
Enum Member Enum Member Description MovePoint Move Point Motion EditSegment Edit Segment Motion -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-