EditPointBuilderEditsegmenttype Enumeration¶
NXOpen.MechanicalRouting.EditPointBuilder.Editsegmenttype is an alias for NXOpen.MechanicalRouting.EditPointBuilderEditsegmenttype
-
class
NXOpen.MechanicalRouting.
EditPointBuilderEditsegmenttype
¶ Bases:
object
Specifies the options available for Edit Segment motion.
Enum Members
Enum Member Enum Member Description NotSet Move Point Motion Length Edit length type in Edit Segment Motion Angle Edit angle type in Edit Segment Motion -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-