DynamicCutElbowBehaviorBuilder Class¶
-
class
NXOpen.MechanicalRouting.
DynamicCutElbowBehaviorBuilder
¶ Bases:
NXOpen.Builder
Represents
NXOpen.MechanicalRouting.DynamicCutElbowBehaviorBuilder
.To create a new instance of this class, use
NXOpen.MechanicalRouting.BuilderFactory.CreateDynamicCutElbowBehaviorBuilder()
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
IsLockedCutElbow | Returns true if the current model element is Cut Elbow and is Locked State for Dynamic behavior for Cut Elbow. |
SetLockedCutElbow | Sets true to define the locked state for dynamic behavior. |
SetModelElementRevision | Sets NXOpen.PDM.ModelElementRevision of Routing Reuse type. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
IsLockedCutElbow¶
-
DynamicCutElbowBehaviorBuilder.
IsLockedCutElbow
¶ Returns true if the current model element is Cut Elbow and is Locked State for Dynamic behavior for Cut Elbow.
Signature
IsLockedCutElbow()
Returns: Return type: bool New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
SetLockedCutElbow¶
-
DynamicCutElbowBehaviorBuilder.
SetLockedCutElbow
¶ Sets true to define the locked state for dynamic behavior.
If set false this will have the dynamic behavior. If the current model design element is not a cut elbow this will will be ignored.
Signature
SetLockedCutElbow(lockState)
Parameters: lockState (bool) – New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
SetModelElementRevision¶
-
DynamicCutElbowBehaviorBuilder.
SetModelElementRevision
¶ Sets
NXOpen.PDM.ModelElementRevision
of Routing Reuse type.Raise an error if passed other type of object.
Signature
SetModelElementRevision(modelElementRevision)
Parameters: modelElementRevision ( NXOpen.PDM.ModelElementRevision
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
DynamicCutElbowBehaviorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.