ConnectivityService Class¶
-
class
NXOpen.MechanicalRouting.
ConnectivityService
¶ Bases:
object
Represents a
NXOpen.MechanicalRouting.ConnectivityService
object.Use the
MechanicalRouting.RoutingManager.ConnectivityService()
to obtain an instance of this class.To obtain an instance of this class, refer to
NXOpen.MechanicalRouting.RoutingManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
GetConnectedPorts | Returns the pairs of connected ports in the subset. |
GetPortsConnectedToDesignElement | Returns the pairs of ports connected to the given Design Element. |
Method Detail¶
GetConnectedPorts¶
-
ConnectivityService.
GetConnectedPorts
¶ Returns the pairs of connected ports in the subset.
Signature
GetConnectedPorts(part)
Parameters: part ( NXOpen.Part
) – The subset part.Returns: a tuple Return type: A tuple consisting of (connectedPorts1, connectedPorts2). connectedPorts1 is a list of NXOpen.Routing.Port
. connectedPorts2 is a list ofNXOpen.Routing.Port
.New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
GetPortsConnectedToDesignElement¶
-
ConnectivityService.
GetPortsConnectedToDesignElement
¶ Returns the pairs of ports connected to the given Design Element.
Signature
GetPortsConnectedToDesignElement(part)
Parameters: part ( NXOpen.Assemblies.Component
) – The component of the Design Element.Returns: a tuple Return type: A tuple consisting of (connectedPorts1, connectedPorts2). connectedPorts1 is a list of NXOpen.Routing.Port
. connectedPorts2 is a list ofNXOpen.Routing.Port
.New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)