MeasurementDeviationReportType Enumeration¶
NXOpen.Measurement.DeviationReportType is an alias for NXOpen.MeasurementDeviationReportType
-
class
NXOpen.
MeasurementDeviationReportType
¶ Bases:
object
Describes type of the ‘Deviation Checking’ report.
Enum Members
Enum Member Enum Member Description NoDeviation No Deviation AllDeviation All Deviation MaximumDistance Maximum Distance MinimumDistance Minimum Distance MaximumAngle Maximum Angle MinimumAngle Minimum Angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-