MeasureRectangularExtreme Class¶
-
class
NXOpen.
MeasureRectangularExtreme
¶ Bases:
NXOpen.GenericMeasure
Represents a rectangular extreme point measurement
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
MeasurementType | Returns the type of the measurement |
Point | Returns the centroid point of the measurement |
Methods¶
Method | Description |
---|---|
CreateFeature | Creates and returns a measurement feature |
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Property Detail¶
Point¶
-
MeasureRectangularExtreme.
Point
¶ Returns the centroid point of the measurement
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point3d
New in version NX8.5.0.
License requirements: None.
Method Detail¶
CreateFeature¶
-
MeasureRectangularExtreme.
CreateFeature
¶ Creates and returns a measurement feature
Signature
CreateFeature()
Returns: Return type: NXOpen.Measure
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)