MeasureLength Class¶
-
class
NXOpen.
MeasureLength
¶ Bases:
NXOpen.SingleMeasure
Represents a single valued length measurement
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
MeasurementType | Returns the type of the measurement |
Value | Returns the value of the measurement |
Methods¶
Method | Description |
---|---|
CreateEmbedded | Creates and returns an embedded measurement expression. |
CreateEmbeddedObject | Creates an embedded measurement. |
CreateFeature | Creates and returns a measurement feature |
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Method Detail¶
CreateEmbedded¶
-
MeasureLength.
CreateEmbedded
¶ Creates and returns an embedded measurement expression.
Deprecated: Use CreateEmbeddedObject instead
Signature
CreateEmbedded()
Returns: Return type: str New in version NX4.0.0.
Deprecated since version NX5.0.1: Use
MeasureLength.CreateEmbeddedObject()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
CreateEmbeddedObject¶
-
MeasureLength.
CreateEmbeddedObject
¶ Creates an embedded measurement.
The name of the measurement can be used in an expression formula.
Signature
CreateEmbeddedObject()
Returns: a tuple Return type: A tuple consisting of (measurement, name). measurement is a NXOpen.Scalar
. the measurement name is a str. the name of the measurementNew in version NX5.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFeature¶
-
MeasureLength.
CreateFeature
¶ Creates and returns a measurement feature
Signature
CreateFeature()
Returns: Return type: NXOpen.Measure
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)