MaterialUtilitiesStressStrainData Enumeration¶
NXOpen.MaterialUtilities.StressStrainData is an alias for NXOpen.MaterialUtilitiesStressStrainData
-
class
NXOpen.
MaterialUtilitiesStressStrainData
¶ Bases:
object
The stress strain data type
Enum Members
Enum Member Enum Member Description EngineeringStressEngineeringStrain Engineering stress-Engineering strain EngineeringStressEngineeringPlasticStrain Engineering stress-Engineering plastic strain TrueStressLogStrain True stress-log strain TrueStressLogPlasticStrain True stress-log plastic strain Undefined Undefined type - data is assumed to be defined using the type used by the solver, no attempt will be made to convert the data to the type the solver requires -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-