LoadOptionsParent Enumeration¶
NXOpen.LoadOptions.Parent is an alias for NXOpen.LoadOptionsParent
-
class
NXOpen.
LoadOptionsParent
¶ Bases:
object
Options to allow you to specify how unloaded parents should be loaded when interpart data loading is turned on
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description Partial Do not load any unloaded parents, but fully load partially loaded parts with parent geometry. Immediate Fully load parts that satisfy one level of parent references as well as any partially loaded parts with parent geometry. All Recursively fully load all parts with parent geometry linked to geometry in the parts selected for loading -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-