LoadOptionsLoadOption Enumeration¶
NXOpen.LoadOptions.LoadOption is an alias for NXOpen.LoadOptionsLoadOption
-
class
NXOpen.
LoadOptionsLoadOption
¶ Bases:
object
Option to control how much data is loaded from parts. The first four settings are equivalent to the four possible combinations of the properties
NXOpen.LoadOptions.UsePartialLoading()
andNXOpen.LoadOptions.UseLightweightRepresentations()
. The final setting is reserved for future use.New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description FullyLoad partial load : off, use lightweight : off PartiallyLoad partial load : on, use lightweight : off FullyLoadLightweightDisplay partial load : off, use lightweight : on PartiallyLoadLightweightDisplay partial load : on, use lightweight : on MinimalLoadVisualize reserved for future use -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-