LoadOptionsLoadMethod Enumeration¶
NXOpen.LoadOptions.LoadMethod is an alias for NXOpen.LoadOptionsLoadMethod
-
class
NXOpen.
LoadOptionsLoadMethod
¶ Bases:
object
Options for specifying how to load component parts
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description AsSaved use same directory in which they were saved FromDirectory use same directory as the parent assembly SearchDirectories use a list of search directories -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-