LoadOptionsLoadComponents Enumeration¶
NXOpen.LoadOptions.LoadComponents is an alias for NXOpen.LoadOptionsLoadComponents
-
class
NXOpen.
LoadOptionsLoadComponents
¶ Bases:
object
Options for specifying what component parts to load during part open
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description All load all components NotSet load none of the components LastSet use same set of components as when the assembly was last saved LastFilter use same filter used to last load the assembly SpecifyFilter display list of pre-defined component groups to select from -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-