ListingWindowDeviceType Enumeration¶
NXOpen.ListingWindow.DeviceType is an alias for NXOpen.ListingWindowDeviceType
-
class
NXOpen.
ListingWindowDeviceType
¶ Bases:
object
Describes the type of listing window
Enum Members
Enum Member Enum Member Description Window The UI’s Information window File Output is written to a file instead of the Information window FileAndWindow Output is written to a file and to the Information window NotSet Output is not written anywhere; output gets discarded -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-