ListCreator Class¶
-
class
NXOpen.
ListCreator
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.ListCreator
to be used when exporting the JT Data This class is created usingNXOpen.PvtransManager
.NULL object will be returned from Commit()
To create a new instance of this class, use
NXOpen.JtCreator.NewLevel()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AdvCompression | Returns or sets the m_advCompression * - Specifies the advanced compression for Defined Level of Detail |
Angular | Returns or sets the m_angular * - Specifies the angular tolerance for Defined Level of Detail |
Chordal | Returns or sets the m_chordal * - Specifies the chordal tolerance for Defined Level of Detail |
FeatureSuppression | Returns or sets the m_featureSuppression * - Specifies the feature supression for Defined Level of Detail |
Label | Returns or sets the m_label * - Specifies the label for Defined Level of Detail |
Length | Returns or sets the m_length * - Specifies the length tolerance for Defined Level of Detail |
NxLabel | Returns or sets the m_nxlabel * - Specifies the label for Level of Detail using NX resolution |
Resolution | Returns or sets the m_resolution * - Specifies the resolution type for Level of Detail using NX resolution |
Simplify | Returns or sets the m_simplify * - Specifies the simplification tolerance for Defined Level of Detail |
Tag | Returns the Tag for this object. |
TessOption | Returns or sets the m_tessOption * - Specifies the type for Level of Details, whether Defined Level or Use NX Resolution |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ListCreatorResolutionType Enumeration | resolution Type |
ListCreatorTessellationOption Enumeration | Tessellation Option |
Property Detail¶
AdvCompression¶
-
ListCreator.
AdvCompression
¶ Returns or sets the m_advCompression * - Specifies the advanced compression for Defined Level of Detail
-------------------------------------
Getter Method
Signature
AdvCompression
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvCompression
Parameters: compression (float) – New in version NX8.5.0.
License requirements: None.
Angular¶
-
ListCreator.
Angular
¶ Returns or sets the m_angular * - Specifies the angular tolerance for Defined Level of Detail
-------------------------------------
Getter Method
Signature
Angular
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Angular
Parameters: angular (float) – New in version NX8.5.0.
License requirements: None.
Chordal¶
-
ListCreator.
Chordal
¶ Returns or sets the m_chordal * - Specifies the chordal tolerance for Defined Level of Detail
-------------------------------------
Getter Method
Signature
Chordal
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Chordal
Parameters: chordal (float) – New in version NX8.5.0.
License requirements: None.
FeatureSuppression¶
-
ListCreator.
FeatureSuppression
¶ Returns or sets the m_featureSuppression * - Specifies the feature supression for Defined Level of Detail
-------------------------------------
Getter Method
Signature
FeatureSuppression
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureSuppression
Parameters: suppression (float) – New in version NX8.5.0.
License requirements: None.
Label¶
-
ListCreator.
Label
¶ Returns or sets the m_label * - Specifies the label for Defined Level of Detail
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (str) – New in version NX8.5.0.
License requirements: None.
Length¶
-
ListCreator.
Length
¶ Returns or sets the m_length * - Specifies the length tolerance for Defined Level of Detail
-------------------------------------
Getter Method
Signature
Length
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length
Parameters: length (float) – New in version NX8.5.0.
License requirements: None.
NxLabel¶
-
ListCreator.
NxLabel
¶ Returns or sets the m_nxlabel * - Specifies the label for Level of Detail using NX resolution
-------------------------------------
Getter Method
Signature
NxLabel
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NxLabel
Parameters: label (str) – New in version NX8.5.0.
License requirements: None.
Resolution¶
-
ListCreator.
Resolution
¶ Returns or sets the m_resolution * - Specifies the resolution type for Level of Detail using NX resolution
-------------------------------------
Getter Method
Signature
Resolution
Returns: Return type: NXOpen.ListCreatorResolutionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Resolution
Parameters: resolution ( NXOpen.ListCreatorResolutionType
) –New in version NX8.5.0.
License requirements: None.
Simplify¶
-
ListCreator.
Simplify
¶ Returns or sets the m_simplify * - Specifies the simplification tolerance for Defined Level of Detail
-------------------------------------
Getter Method
Signature
Simplify
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Simplify
Parameters: simplify (float) – New in version NX8.5.0.
License requirements: None.
TessOption¶
-
ListCreator.
TessOption
¶ Returns or sets the m_tessOption * - Specifies the type for Level of Details, whether Defined Level or Use NX Resolution
-------------------------------------
Getter Method
Signature
TessOption
Returns: Return type: NXOpen.ListCreatorTessellationOption
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TessOption
Parameters: tessOption ( NXOpen.ListCreatorTessellationOption
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ListCreator.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.