LinkedMirrorPartEntityMapData Class¶
-
class
NXOpen.
LinkedMirrorPartEntityMapData
¶ Bases:
NXOpen.TaggedObject
JA interface for LinkedMirrorPartEntityMapData oject
This cannot be created
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
AddToMap | Add a map between an entity in the source part and an entity in the mirror part |
GetMappedMirrorPartEntities | The list of mapped entities in the mirror part |
GetMappedSourcePartEntities | The list of mapped entities in the source part |
GetMirrorPartEntitiesToMap | The list of entities in the mirror part that are yet to be mapped |
GetSourcePartEntitiesToMap | The list of entities in the source part that are yet to be mapped |
Method Detail¶
AddToMap¶
-
LinkedMirrorPartEntityMapData.
AddToMap
¶ Add a map between an entity in the source part and an entity in the mirror part
Signature
AddToMap(sourceEntity, mirrorEntity)
Parameters: - sourceEntity (
NXOpen.TaggedObject
) – - mirrorEntity (
NXOpen.TaggedObject
) –
New in version NX8.5.0.
License requirements: None.
- sourceEntity (
GetMappedMirrorPartEntities¶
-
LinkedMirrorPartEntityMapData.
GetMappedMirrorPartEntities
¶ The list of mapped entities in the mirror part
Signature
GetMappedMirrorPartEntities()
Returns: the reference of a user defined feature Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
GetMappedSourcePartEntities¶
-
LinkedMirrorPartEntityMapData.
GetMappedSourcePartEntities
¶ The list of mapped entities in the source part
Signature
GetMappedSourcePartEntities()
Returns: the reference of a user defined feature Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
GetMirrorPartEntitiesToMap¶
-
LinkedMirrorPartEntityMapData.
GetMirrorPartEntitiesToMap
¶ The list of entities in the mirror part that are yet to be mapped
Signature
GetMirrorPartEntitiesToMap()
Returns: the reference of a user defined feature Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
GetSourcePartEntitiesToMap¶
-
LinkedMirrorPartEntityMapData.
GetSourcePartEntitiesToMap
¶ The list of entities in the source part that are yet to be mapped
Signature
GetSourcePartEntitiesToMap()
Returns: the reference of a user defined feature Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.