LinkedMirrorPartBuilderMirrorCsysOption Enumeration¶
NXOpen.LinkedMirrorPartBuilder.MirrorCsysOption is an alias for NXOpen.LinkedMirrorPartBuilderMirrorCsysOption
-
class
NXOpen.
LinkedMirrorPartBuilderMirrorCsysOption
¶ Bases:
object
type of mirror of CSYS The first two axes are mirrored, and the third one is derived from the two mirrored axes using the right hand convention
Enum Members
Enum Member Enum Member Description MirrorXYAndDeriveZ MirrorYZAndDeriveX MirrorXZAndDeriveY -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-