LinkedMirrorPartAttributeEditData Class¶
-
class
NXOpen.
LinkedMirrorPartAttributeEditData
¶ Bases:
NXOpen.TaggedObject
JA interface for LinkedMirrorPartAttributeEditData object
This cannot be created
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
MirrorPart | Returns the mirror part |
SourcePart | Returns the source part |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
MirrorPart¶
-
LinkedMirrorPartAttributeEditData.
MirrorPart
¶ Returns the mirror part
-------------------------------------
Getter Method
Signature
MirrorPart
Returns: the reference of a user defined feature Return type: NXOpen.Part
New in version NX8.5.0.
License requirements: None.
SourcePart¶
-
LinkedMirrorPartAttributeEditData.
SourcePart
¶ Returns the source part
-------------------------------------
Getter Method
Signature
SourcePart
Returns: the reference of a user defined feature Return type: NXOpen.Part
New in version NX8.5.0.
License requirements: None.