LineWidthOption Enumeration¶
-
class
NXOpen.
LineWidthOption
¶ Bases:
object
the line width options. This is used in conjunction with
NXOpen.LineWidthBuilder
Enum Members
Enum Member Enum Member Description Assigned Width value can be obtained from the builder. For example, NXOpen.LineWidthBuilder.Width()
Default Default width. The builder interprets this option as per its need. NoChange Do not modify the width. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-